Setting the device control

Using the Wiser Home app, you can set the control type such as Relay or OpenTherm.
To set the control type:
  1. On the Home screen, tap .
  2. Tap Devices > Boiler Relay > Control Type (A) to select given option:
    • Relay
    • OpenTherm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?