Showing 291 - 300 of 1,622 results

Page 30 of 163
  • Seasonal Comfort Mode

    Wiser Home – System User Guide (Germany, Austria)

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode If you have a shutter control devices installed at your home, Seasonal Comfort Mode feature will be available. Seasonal Comfort Mode is a smart feature helps maintain the perfect temperature throughout the year by automatically
  • Mode Confort Saisonnier

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Mode Confort Saisonnier Mode Confort Saisonnier Mode Confort Saisonnier Le mode Confort Saisonnier utilise la température prévue d’un lieu ou les informations des capteurs de lumière et de température pour déterminer la température d’une pièce et y maintenir une température souhaitée en ouvrant ou
  • Seasonal Comfort Mode

    Wiser Home – System User Guide (Denmark)

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode If you have a shutter control devices installed at your home, Seasonal Comfort Mode feature will be available. Seasonal Comfort Mode is a smart feature helps maintain the perfect temperature throughout the year by automatically
  • Seasonal Comfort Mode

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode The seasonal comfort mode uses the predicted temperature of a location or information from the light and temperature sensors to determine the temperature of a room and maintain a desired temperature in it by opening or closing the
  • Seasonal Comfort Mode

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode The seasonal comfort mode uses the predicted temperature of a location or information from the light and temperature sensors to determine the temperature of a room and maintain a desired temperature in it by opening or closing the
  • Mode Confort Saisonnier

    Odace - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Mode Confort Saisonnier Mode Confort Saisonnier Mode Confort Saisonnier Le mode Confort Saisonnier utilise la température prévue d’un lieu ou les informations des capteurs de lumière et de température pour déterminer la température d’une pièce et y maintenir une température souhaitée en ouvrant ou
  • Wiser Home System User Guide (Germany, Austria)

    desiredtemperature and activate boost mode. To be completed with a Connected Thermostat Insert. Instruction Sheet Device User Guide (With 2A Insert) Device User Guide (With 16A Insert) Connected Thermostat Insert2 A MEG5777-0000 Control water-based heating and cooling applications,such as water-based
  • Wiser Underfloor Heating Controller / Connection Strip Wiser Home Device user guide

    boost time. After the boost time is over, theset-point temperature returns to the current scheduled event or to theprevious set-point temperature. • Moving the slider control to the bottom of the bar activates FrostProtection mode. In this mode, the system maintains the roomtemperature at a constant 5
  • Climatiseur Airzone Plénum et Aidoo Pro Guide de l'utilisateur de l’appareil Wiser Home

    . Pour plusd’informations sur les différents modes, reportez-vous à Boost Mode. – Mode auto :(Ce mode n’est disponible que pour Aidoo) Permet lacommutation automatique entre le refroidissement et le chauffage et peuts’éteindre si nécessaire. IMPORTANT: Le mode auto peut être activé uniquement
  • Google Home

    Wiser Home – System User Guide (Spain and Portugal)

    new setpoint temperature to the prior setpoint ± 3 degrees. This value is controlled by Google Home and differs from a normal Wiser boost, which defaults the new setpoint to ±2 degrees above/below the current ambient temperature. Commands for turning the heating “ON/ OFF” are currently unavailable on
Page 30 of 163