Showing 3,631 - 3,640 of 9,859 results

Page 364 of 986
  • Google Home

    Wiser Home – System User Guide (Spain and Portugal)

    Google Home Google Home Google Home Google Home is a brand of smart speakers that work similarly to Amazon Echo. Google’s intelligent PA, Google Assistant, is equivalent to Amazon’s Alexa. Google Home is also available on all Android devices and does not require the use of the ‘Smart Speakers’. The
  • Pairing the device with the Wiser Hub

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address
  • Manual sensor settings

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Manual sensor settings Manual sensor settings Manual sensor settings A thermostat with a preset value of P6 to P8 can be connected to an external floor sensor. This enhances the user's experience in regulating the temperature. After selecting a preset, press O button for 1 second to confirm. The
  • LED Indications

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    thermostat matrix display flashes a green LED when the thermostat successfully joins a network. Fails to join the network The thermostat matrix display flashes a red LED when the thermostat fails to join the network. Presetting the device Status User Interaction Description Enter preset selection
  • Configuring the seasonal comfort mode

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    configuring the seasonal comfort mode. Define the orientation in which the shutters are installed at home: Select the orientation in which each shutter is installed at home and tap Next. If any shutter is covering a door, tap Yes I have shutters over a door. If no shutter is covering a door or you have an
  • Configuring the seasonal comfort mode

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    configuring the seasonal comfort mode. Define the orientation in which the shutters are installed at home: Select the orientation in which each shutter is installed at home and tap Next. If any shutter is covering a door, tap Yes I have shutters over a door. If no shutter is covering a door or you have an
  • Emparelhar o interruptor sem fios com o módulo de botão de pressão

    Sistema M e Sistema D - Botão de pressão conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    Emparelhar o interruptor sem fios com o módulo de botão de pressão Emparelhar o interruptor sem fios com o módulo de botão de pressão Emparelhar o interruptor sem fios com o módulo de botão de pressão Prima ligeiramente a parte superior do botão de pressão 5 vezes numa sequência rápida no
  • Lights

    Wiser Home – System User Guide (France)

    Lights Lights Lights Not all Devices can be added to all Wiser Hubs. To find out if a Device can be added to your Hub, please check chapter Device compatibility list Connected Relay Switch 10A S5x0530W Switch ohmic, inductive or capacitive loads. Instruction Sheet (PDF) Device User Guide Connected
  • Pairing the device with the Wiser Hub

    Odace - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The
  • Pairing the device with the Wiser Hub

    Unica - Connected Motion Sensor with Dimmer LED – Wiser Home Device user guide

    incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid. (B): Tap this option if you
Page 364 of 986