Manual sensor settings
Selecting floor sensor type
After selecting a preset, the thermostat enters the Floor Sensor Selection menu. In this menu, you can manually choose the sensor type connected to the thermostat. This allows the thermostat to convert and display the temperature accurately.
To select the floor sensor type:
-
When the selection menu opens, 10 appears on the thermostat’s dot-matrix display.
-
Press the + or – touch button to scroll through the available sensor types:
-
10 kOhm
-
12 kOhm
-
15 kOhm
-
33 kOhm
-
47 kOhm
TIP: When + button is pressed, sensor type 10 becomes 12, continue to press the + button, and the type changes to 15, 33, and 47.
When – button is pressed, sensor type 47 becomes 33, continue to press the – button, and the type changes to 15, 12, and 10. -
-
Select the sensor type which is installed and then press the O touch button for a few seconds to confirm the selection.
-
The thermostat dot-matrix display the sensor type and
LED flashes blue.
Setting temperature calibration
After selecting the floor sensor type, you must set the calibration value (offset value) of the sensor in order to minimize any variation in temperature measurement.
To set temperature calibration:
-
Press + or – touch button on the device to set the calibration value..
NOTE: The temperature calibration ranges from -9°C to +9°C and can be adjusted in 0.5°C increments. -
Set the calibration value, press the O touch button for a few seconds to confirm the selection.
-
The thermostat dot-matrix display calibration value and
LED flashes purple.
Setting maximum guard temperature
After
setting temperature calibration, you must set the maximum guard temperature.
It is the upper limit of the floor sensor.
Minimum
guard temperature can only be set through Wiser Home app.
To set maximum guard temperature:
-
Press + or – touch button on the device to set the maximum limit.
NOTE: The temperature limit ranges from 11°C to 40°C. -
Set the value, press the O touch button for a few seconds to confirm the selection.
-
The thermostat dot-matrix display calibration value and
LED flashes red.
-
If you want to update the sensor settings manually after setting up the device, Press O and + button simultaneously to enter preset selection and press O to confirm preset and enter sensor setting.
-
You can also perform a factory reset to remove all settings and configure the thermostat newly. Refer resetting the device.
-
It is possible to modify or update sensor settings without resetting the thermostat with the Wiser Home app. Refer Using the device.