Showing 371 - 380 of 1,457 results

Page 38 of 146
  • Troubleshooting in Quick Home Connect

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    module shades control Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Micro module shades
  • Setting boost mode manually

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Setting boost mode manually Setting boost mode manually Setting boost mode manually You can enable and disable boost mode manually.When enabled the temperature increases by 2° C for temperature control modes and by +2 over the setpoint. To enable boost mode: Press the rotary push-button until the
  • Selecting the operating mode

    Wiser Window/Door Sensor – Wiser Home Device user guide

    Selecting the operating mode Selecting the operating mode Selecting the operating mode Using the Wiser Home app, you can select the operating mode for the sensor such as window or door. On the Home screen, tap icon. Tap Devices Window/Door Sensor Operation Mode (A) to select one of the following
  • Mode silencieux de l’appareil

    Wiser détecteur de fumée connecté sur secteur 230V – Guide de l'utilisateur de l’appareil Wiser Home

    Mode silencieux de l’appareil Mode silencieux de l’appareil Mode silencieux de l’appareil Désactiver les détecteurs de fumée Lors d’un événement d’alarme, identifiez d’abord les détecteurs de fumée qui ont détecté de la fumée, ceux-ci auront des LED rouges clignotants. Appuyez ensuite brièvement
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    dimmer The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Rotary dimmer The Wireless switch
  • Wiser Motion Sensor Wiser Home Device user guide

    triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. e.g. Good
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    -button switch The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button switch The
  • Troubleshooting in Quick Home Connect

    LK One Wiser Push-button Switch – Wiser Home Device user guide

    -button switch The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button switch The
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Multiwire LED Push-button Dimmer – Wiser Home Device user guide

    -button dimmer The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button dimmer The
  • Troubleshooting in Quick Home Connect

    LK One Wiser Multiwire LED Rotary Dimmer – Wiser Home Device user guide

    dimmer The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Rotary dimmer The Wireless switch
Page 38 of 146