DUG_Window/Door Sensor_WH-06

Selecting the operating mode

Using the Wiser Home app, you can select the operating mode for the sensor such as window or door.
  1. On the Home screen, tap icon.
  2. Tap Devices > Window/Door Sensor > Operation Mode (A) to select one of the following option (B):
    • Window

    • Door

    TIP: Additionally, you can select the operating mode of the sensor by tapping on the Control tab Window/Door Sensor > Device settings > Operation mode (A).
NOTE:
  • In operation mode "Window," the Control tab displays a Window Sensor (C).

  • In operation mode "Door," the Control tab displays a Door Sensor (D).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?