Showing 441 - 450 of 1,457 results

Page 45 of 146
  • Configuring the seasonal comfort mode

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    Configuring the seasonal comfort mode Configuring the seasonal comfort mode Configuring the seasonal comfort mode Using the Wiser Home app, you can configure the seasonal comfort mode to define the desired temperature and location of the shutters and sensors in the home. Pre-requisite: Shutters
  • Troubleshooting in Quick Home Connect

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    module light switch Micro module shades control Multiwire micro module dimmer Push–button dimmer Socket outlet Relay switch Blind control switches Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in
  • Wiser Home

    Modes Modes Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Boost Mode Boost Mode Schneider Electric 35 rue Joseph Monier
  • Wiser Home

    Schedule Deleting a Schedule Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Modes Modes Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph
  • Sensor de temperatura/humedad Wiser Guía del usuario del dispositivo Wiser Home

    when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. SUGERENCIA: Away mode can also be used as a trigger to turn offthe lights, dimmer
  • LK FUGA® - Wiser wireless socket outlet 1½ M Wiser Home Device user guide

    motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout , refer to the system user guide. NOTE: Maximum 10 conditions can be added. New automation If When Conditions are met All conditions Start by
  • Override modes

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    Override modes Override modes Override modes This mode temporarily overrides the automatic operation of the motion sensor. For example, it allows you to trigger the load for a set period, even if no motion is detected. The motion sensor has two modes that can temporarily override the default
  • Wiser Home

    Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Modes Modes Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0
  • Modes manuels

    Capteur de mouvement extérieur ARGUS 360 – Guide de l'utilisateur de l’appareil Wiser Home

    Modes manuels Modes manuels Modes manuels Ce mode remplace temporairement le fonctionnement automatique du capteur de mouvement. Par exemple, il vous permet de déclencher la charge pendant une période définie, même si aucun mouvement n'est détecté. Le capteur de mouvement a deux modes pouvant
  • LED indications

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing User Action LED Indication Status Press the Setup/Reset button 3 times Status LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, status LED glows green for some time before turning Off
Page 45 of 146