DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Override modes

This mode temporarily overrides the automatic operation of the motion sensor. For example, it allows you to trigger the load for a set period, even if no motion is detected. The motion sensor has two modes that can temporarily override the default automatic mode. These modes are activated by switching the sensor OFF and then back ON using a switch or push-button.
NOTE:
  • The automatic mode is the normal use mode where the motion sensor is in ON state.

  • This mode is not applicable in the Wiser Home app.

  • During mode 1 and mode 2, the lux value adjustments are disabled.

Mode 1 :

The connected load turns ON or OFF depending on its current state for the set time. After the set time expires, the sensor returns to automatic mode.

To trigger mode 1: Turn the switch or push-button OFF - ON within 1 s.

Example 1: Auto Load OFF

Example 2: Auto Load ON

To manually exit mode 1: Switch to mode 2 (power OFF - ON twice within 2 s), then power OFF-ON within 1 s.

Mode 2:

The connected load stays ON for four hours. After four hours, the sensor returns to automatic mode.

NOTE: When the mode 2 is active, turning the switch or push-button OFF - ON twice again within 2 s will turn on the load for another 4 hours.

To trigger mode 2: Turn the switch or push-button OFF - ON twice within 2 s.

Example:

To manually exit mode 2: Power OFF-ON within 1s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?