Showing 4,631 - 4,640 of 9,846 results

Page 464 of 985
  • Emparelhar o interruptor sem fios com o micromódulo persianas (Relé)

    Micromódulo Estores Wiser – Guia do utilizador do dispositivo Wiser Home

    Emparelhar o interruptor sem fios com o micromódulo persianas (Relé) Emparelhar o interruptor sem fios com o micromódulo persianas (Relé) Emparelhar o interruptor sem fios com o micromódulo persianas (Relé) Prima ligeiramente a parte superior do botão de pressão 5 vezes numa sequência rápida no
  • Configuration d’un programme

    Unica - Prise de courant connectée 16A – Guide de l'utilisateur de l’appareil Wiser Home

  • Example of an automation

    PowerTag Control – Device user guide

    Example of an automation Example of an automation Example of an automation This demonstration shows you how to create an automation to controlling a hot water system when solar production is greater than 2 kW. If your home location is in Belgium, Denmark, Sweden, and Finland. Make sure to install
  • Updating the firmware

    Wiser Home – System User Guide (Sweden, Finland)

    Updating the firmware Updating the firmware Updating the firmware When the hub is connected to the Wiser cloud, it automatically updates the latest firmware. For the first time installation, if you want to check and update the firmware manually, use the app as a professional installer. To check and
  • eSetup App

    Wiser Home – System User Guide (Sweden, Finland)

    . This dedicated application for Electricians is a commissioning tool for Wiser devices in residential and SmartLink, Powertag devices in Small Buildings. Not all the wiser devices can be configured using the eSetup app. The app offer the configuration for devices such as Light and Shutter Devices
  • Hub

    Wiser Home – System User Guide (UK, Ireland)

    , according to your heating system One Channel (WT714R1S0902): 1x heating, for combination boilers. Two Channels (WT724R1S0902): 1x Heating, 1x Hot water, for conventional boilers with a separate hot water cylinder Three Channels (WT734R1S0902): 2x Heating, 1x Hot water, for large properties with
  • Pairing 1-gang with 1 or 2 Blind Control Switches

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Pairing 1-gang with 1 or 2 Blind Control Switches Pairing 1-gang with 1 or 2 Blind Control Switches Pairing 1-gang with 1 or 2 Blind Control Switches If you want to pair a 1-gang Wireless switch with one blind control switch, follow the steps up to step 2. To continue with a second blind control
  • Setting the room temperature using the app

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Setting the room temperature using the app Setting the room temperature using the app Setting the room temperature using the app Using the Wiser Home app, you can adjust the room temperature. To adjust the room temperature: On the Control tab, tap All devices or a room tab where the thermostat is
  • Informações de segurança

    Sistema M e Sistema D - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    especiais podem aparecer ao longo deste manual ou no equipamento para avisar de potenciais perigos ou para chamar a atenção para informação que esclareça ou simplifique um procedimento. O aditamento de um dos símbolos a um rótulo de segurança «Perigo» ou «Aviso» indica a existência de um perigo elétrico que
  • Micromódulo persianas (Relé)

    Sistema M e Sistema D - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    Micromódulo persianas (Relé) Micromódulo persianas (Relé) Micromódulo persianas (Relé) Prima ligeiramente a parte superior do botão de pressão 5 vezes numa sequência rápida no interruptor sem fios. O LED de estado pisca a verde. PERIGO DE CHOQUE ELÉTRICO Cumpra os regulamentos ao trabalhar em peças
Page 464 of 985