Showing 6,591 - 6,600 of 9,846 results

Page 660 of 985
  • Shutter Calibration without Wiser app

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    the rocker, you can use either top or bottom push-button. Press bottom and top push-buttons for 3 seconds. The status LED blinks green. If the shutter is not in a completely open position, it starts to open and reaches the top position. In this step, If the shutter is already in the open position
  • Shutter calibration with Wiser app

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    percentage (A). The shutter opens completely and then it reaches to the desired position set in step 2. The shutter is now calibrated. Shutter with tilting slats On the Control tab, tap All devices or the room tab where the device is located. On the device control screen, in the Position tab, drag the
  • Använda enheten

    EVlink Home Smart – Användarhandbok för Wiser Home-enhet

    Använda enheten Använda enheten Använda enheten Med hjälp av kontrollpanelen kan du starta och stoppa laddningen och övervaka strömförbrukningen. På sidan Kontroll trycker du på EVlink Home Smart för att komma till kontrollpanelen. På sidan för kontrollpanelen, Du kan se alternativen A, B, C, D
  • Using the device

    Mureva EVlink – Wiser Home Device User Guide

    Using the device Using the device Using the device The Control Panel allows you to start and stop charging and monitor the power consumption. On the Control page, tap Mureva EVlink Socket to access the control panel. On the control panel page, You can see the options A, B, C, D. Tap to see the
  • Support

    Wiser Home – System User Guide (Spain and Portugal)

    of the Wiser system. Upload Logs This option allows you to upload log files if you have identified any issues in the app. When you tap on the option, a popup will appear, allowing you to describe the issue. Click OK to generate an ID number for this problem, and then contact the Schneider support
  • About the device

    Schneider Charge – Wiser Home Device user guide

    elements A Charging station The charging station provides electrical energy to electric vehicles that are plugged into the Schneider Charge. B Cable winding trough When not in use, wrap the charging cable around the charging station’s trough to avoid tripping hazards and equipment damage. C Front
  • Support

    Wiser Home – System User Guide (Denmark)

    of the Wiser system. Upload Logs This option allows you to upload log files if you have identified any issues in the app. When you tap on the option, a popup will appear, allowing you to describe the issue. Click OK to generate an ID number for this problem, and then contact the Schneider support
  • Konfigurera UFH-ställdon

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    ihop och tryck sedan på Nästa för att konfigurera golvvärmen. Tryck Utgångsenhet (A) för att öppna rullgardinsmenyn och välj UFH (B) från listan som är ansluten till termostaten. Inbyggt relä är valt som standard som utgångsenhet, det finns inga andra inställningar för det. Tryck på Kanaler (C) och
  • Multiwire Micro Module Dimmer

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    right mechanical push button. If you do not need the lower rocker of the Wireless switch, you can replace it with a blind plate. Remove the top rocker and short press the left push button 5 times in quick succession on the Wireless switch. The status LED blinks green. HAZARD OF ELECTRIC SHOCK
  • Shutter

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    Shutter Shutter Shutter On the Home screen, tap . Tap Devices Shutters. Tap Open duration/ Close duration (A) and enter the recorded shutter opening/closing time.
Page 660 of 985