DUG_Schneider Charge_WH-04

About the device

The Schneider Charge provides homeowners an easy and smart way to charge their electric vehicles. The Wiser Home app enables easy access to monitor and control the charging experience remotely, and schedule charging sessions using renewable energy from solar panels. This helps to optimize the energy consumption, avoid power overruns and reduce the carbon footprint.

When installed with Anti-Tripping Module, Schneider Charge provides an end-to-end solution for power load management. For more information, refer Anti-tripping System.

Operating elements

A

Charging station

The charging station provides electrical energy to electric vehicles that are plugged into the Schneider Charge.

B

Cable winding trough

When not in use, wrap the charging cable around the charging station’s trough to avoid tripping hazards and equipment damage.

C

Front indicator light

Indicates the status of Schneider Charge. Refer LED indication.

D

Side indicator light

Indicates the status during Wi-Fi® access point commissioning and anti-tripping module pairing.

E

Functional button (Push button)

To enable Wi-Fi access point/reset PIN code/anti-tripping module pairing (power off and then switch on the device to enable this button).

F

Charging socket

To plug in your T2 charging cable.

IMPORTANT:
  • Use the Anti-tripping module only with the Schneider Charge. Do not use it with other electrical devices.

  • Pair the Anti-tripping module with Schneider Charge as a standalone product. it prevents the use of PowerTag in the system. Hence, it restricts the functionality of certain features like Wiser Home AI.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?