Showing 7,701 - 7,710 of 9,969 results

Page 771 of 997
  • Removing the device

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    Removing the device Removing the device Removing the device Using the Wiser home app, you can remove the Plug from the Wiser system. On the Home screen, tap . Tap Devices Smart Plug Delete (A). All the network related data will be deleted.
  • Eliminación del dispositivo

    Enchufe inalámbrico Wiser 16A – Guía del usuario del dispositivo Wiser Home

    Eliminación del dispositivo Eliminación del dispositivo Eliminación del dispositivo Con la aplicación Wiser Home, puede eliminar el enchufe del sistema Wiser. En la pantalla de inicio, pulse . Pulse Dispositivos Enchufe inalámbrico Eliminar (A). Se eliminarán todos los datos relacionados con la red.
  • Switching operation using the app

    LK FUGA® - Wiser wireless socket outlet 1½ M – Wiser Home Device user guide

    Switching operation using the app Switching operation using the app Switching operation using the app Using the Wiser Home app, you can turn On/Off the Socket outlet remotely. On the Control tab, tap All and find the device. Tap (A) to turn On/Off the device.
  • Renommer le dispositif

    Wiser Actionneur de Chauffage électrique pour la commande de température – Guide de l’utilisateur de l’appareil

    Renommer le dispositif Renommer le dispositif Renommer le dispositif Vous pouvez renommer le dispositif à l’aide de l’application Wiser Home. Sur l’écran d’ accueil, appuyez sur . Appuyez sur Dispositifs Chauffage Actionneur de chauffage électrique Nom (A) pour renommer e dispositif. Le Type et
  • Troubleshooting

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

  • Fejlfinding

    Wiser 16 A relæ til styring af temperatur – Brugervejledning til enheden

  • Indicações do LED no Quick Home Connect

    Micromódulo Variador Wiser – Guia do utilizador do dispositivo Wiser Home

    Indicações do LED no Quick Home Connect Indicações do LED no Quick Home Connect Indicações do LED no Quick Home Connect Emparelhar o dispositivo no Quick Home Connect Ação do utilizador Indicador LED Estado Prima 5 vezes o botão de pressão numa sequência rápida. O LED pisca a verde uma vez por segundo. O modo de emparelhamento fica ativo durante 60 segundos. Quando o emparelhamento estiver concluído, o LED para de piscar.
  • Setting RL-LED mode

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    Setting RL-LED mode Setting RL-LED mode Setting RL-LED mode You can change the dimming mode in the app if you have problems with light flickering. By changing the dimming mode, the dimming quality is also improved. On the Home screen, tap . Tap Devices Micromodule Dimmer . Tap the toggle switch (A) to enable the RL-LED Mode.
  • Kirkkaustason säätö sovelluksen avulla

    Wiser säädinmoduuli ZB – Wiser Home -laitteen käyttöopas

    ohjaus -näytössä liukupalkkia ylös/alas suurentaaksesi/pienentääksesi kirkkautta (A). Voit myös kytkeä päälle/pois päältä Puck Laitteen ohjausnäytössä, napauta (B) kytkeäksesi päälle/pois päältä.
  • Indstilling af RL-LED-tilstand

    Wiser Puck lysdæmper – Brugervejledning til Wiser Home-enheden

    Indstilling af RL-LED-tilstand Indstilling af RL-LED-tilstand Indstilling af RL-LED-tilstand Du kan ændre dæmpningstilstanden i appen, hvis du har problemer med flimren. Ved at ændre dæmpningstilstanden forbedrer du også dæmpningskvaliteten. Tryk på på Hjem-skærmen. Tryk på Enheder Mikromodullysdæmper . Tryk på vippekontakten (A) for at aktivere RL-LED tilstanden.
Page 771 of 997