Showing 791 - 800 of 9,870 results

Page 80 of 987
  • Wiser Home

    Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Creating a Moment Creating a Moment Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Editing a Moment Editing a Moment Schneider Electric 35 rue Joseph Monier 92500 Rueil
  • Creating an Account

    Wiser Home – System User Guide (Germany, Austria)

    Creating an Account Creating an Account Creating an Account To be able to control the system from your smartphone, you need to create an account and log in. Once the professional installer sets up the Wiser system, they will hand it over to the homeowner. Subsequently, the homeowner will create an
  • Creating an Account

    Wiser Home – System User Guide (Spain and Portugal)

    Creating an Account Creating an Account Creating an Account To be able to control the system from your smartphone, you need to create an account and log in. Once the professional installer sets up the Wiser system, they will hand it over to the homeowner. Subsequently, the homeowner will create an
  • Creating an Account

    Wiser Home – System User Guide (Sweden, Finland)

    Creating an Account Creating an Account Creating an Account To be able to control the system from your smartphone, you need to create an account and log in. Once the professional installer sets up the Wiser system, they will hand it over to the homeowner. Subsequently, the homeowner will create an
  • Criar um momento

    Micromódulo Variador Wiser – Guia do utilizador do dispositivo Wiser Home

    Criar um momento Criar um momento Criar um momento Um momento permite-lhe agrupar várias ações que normalmente são realizadas em conjunto. Através da aplicação Wiser Home, pode criar momentos com base nas suas necessidades. No ecrã Inicial, toque em Momentos . Introduza o nome do momento (A
  • LK FUGA® Wiser wireless PIR dimmer with neutral Wiser Home Device user guide

    usually performed together.By using the Wiser Home app, you can create moments based on your needs. Creating a moment 1. On the Home screen, tap . 2. Go to Moments and tap to create a moment. 3. Enter the name of the moment (A).TIP: You can choose the cover image that represents your moment by
  • Criar um momento

    Controlador/Barra de Conexão de Aquecimento de Piso Radiante Wiser – Guia do utilizador do dispositivo Wiser Home

    Criar um momento Criar um momento Criar um momento Um Momento permite ao utilizador agrupar várias ações que normalmente são executadas em conjunto. Através da aplicação Wiser Home, pode criar momentos com base nas suas necessidades. Para criar um momento: No ecrã Inicial, toque em . Aceda a
  • System M and System D - Connected Thermostat 2 A, ZB Wiser Home Device user guide

    delete Schedule 4. To edit the EVENTS, select a day, and tap to change the time andtemperature. Creating a MomentA Moment allows you to group multiple actions that are usually done together.Using the Wiser app, you can create moments based on your needs (such asmovie night). To create a moment: 1
  • Creación de una programación horaria

    Schneider Charge – Guía del usuario del dispositivo Wiser Home

    estado Encender y Apagado de una programación horaria. Seleccione los días (A). Toque (B) para editar la programación horaria. Seleccione un estado (encendido/apagado) (C), un período de tiempo (D) y toque Aceptar. Puede añadir varias programaciones horarias en función de sus necesidades. Seleccione los
  • Oprettelse af et scenarie

    Wiser rumtermostat – Brugervejledning til Wiser Home-enheden

    at oprette et scenarie. Indtast navnet på scenariet (A). Du kan vælge det forsidebillede, der bedst repræsenterer dit scenarie, ved at trykke på . Tryk på Tilføj handlinger (B) for at vælge listen over enheder. I menuen Tilføj handlinger kan du vælge enhederne (C). Når alle enhederne er valgt, skal
Page 80 of 987