DUG_System M and System D - Wireless Switch_WH-07

Removing configured Action/Moment

You can remove the configured Action or Moment from the Wireless switch key.

To remove the configured Action/Moment:

  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.

  2. Tap push button and tap Action / Moment >Remove > Yes I’m confirm

    to remove configured Action/Moment from the Wireless switch key.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?