Removing the device

Using the Wiser Home app, you can remove the Boiler Relay from the Wiser system.
To remove the Boiler Relay:
  1. On the Home screen, tap .
  2. Tap Devices > Boiler Relay > Delete (A).
  3. In the next screen read the warning and tap Delete.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?