Resetting the device

You can reset the Boiler Relay to factory default mode.

Press and hold the setup button for >20 s.
After 15 seconds, the LED flashes red.

NOTE: The Boiler Relay is removed from the Wiser system and all its function will be inactive until you recommission the device..

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?