For your safety

WARNING
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The wallplate terminals may carry electrical current even when the device is not working. When working on the device always disconnect the device from the supply using the fuse in the incoming circuit.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
RISK OF DAMAGE TO DEVICE
Always operate the product in compliance with the specified technical data.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?