Pairing the main device with On Grid solar system
If you have installed the PowerTag with an existing On Grid solar system, the power flow would be in any of the following directions:
-
Grid to Home: Import
(Home consuming power from Grid) -
Home to Grid: Export
(Excess power from Solar production fed to Grid)
It is necessary to configure the correct power direction else the PowerTag may measure the power direction incorrectly - (Grid to Home as export) and (Home to grid as import).
- On the Home page, tap
.
- Tap Devices >
> Energy.
- Select PowerTag Energy.
- The Device Discovery page will search for a minute to display the available PowerTags.
- If there is more than one device available, select one among them.
- On the Device Configuration page, tap Identify to recognize the main
PowerTag.A notification window is prompted and the status LED flashes fast in green on the PowerTag.
- Tap OK on the notification window when you have finished identifying the PowerTag.
- Tap
to assign a label to the PowerTag.
The label list appears on the Type page. - Select a label type (Grid) and tap Save.NOTE: It is recommended to select the Grid type to represent the main PowerTag.Once the Grid type is selected, by default the Name is assigned as Main Incomer.
- Tap
(A) and select Yes if you have installed solar panels.
The power direction will be enabled automatically. - Tap
(B) and select any one of the options based on your requirement:
- Yes, I sell all of it: (Grid tied solar system) Connected to the Grid (main supply) of the house. All the produced energy is fed into the Grid.
- Yes, I sell some of it: (On Grid solar system) Connected to the Grid (main supply) of the house. If the system produces more energy than is used, the excess power is fed into the Grid.
- No: (Off Grid solar system) Works independently and is not connected to the Grid but have batteries which can store solar power generated by the system.
- Set the Grid Limit/Main Incomer Size (C).NOTE: The Grid Limit / Main Incomer Size refers to the size in Amps of the main switch protecting the switchboard. By default, it is set in Wiser Home at 63 A. It can be set between 15 A and 160 A as required.IMPORTANT: You cannot enter a value that is greater or less than the specified range.
- If you have selected the option as Yes, I sell all of
it and the power direction is from Grid to Home.
- Enable the Reverse Direction toggle switch.
- If you have selected the option as Yes, I sell some
of it.
- Switch off the solar circuit breaker.
If the power direction is from Home to Grid. - Enable the Reverse Direction toggle switch.
- Switch on the solar circuit breaker.
- Switch off the solar circuit breaker.
- If you have selected the option as No, the power direction is Grid to Home. Enable the Reverse Direction toggle switch if the power direction is incorrect.
- Tap Save.
- You will be notified to enter the tariff after the PowerTag
is commissioned, refer to Setting Tariff. NOTE:
-
If you have already configured your tariff, you will be directed to Home page to view the status of device.
-
If PowerTag is installed before installing an On Grid solar system, refer to Advanced settings.
-
If you have configured your PowerTag as Solar or Solar / Battery (combo), (A) field Do you have solar panels? will be disabled. Refer to Pairing the device with ESS.
-