Common questions on interconnection setup
| Scenarios | Required steps for interconnection | |
|---|---|---|
|
I have only 755WSA smoke alarms and Wiser Hub. |
All smoke alarms to be paired to Wiser Hub. |
Follow the steps
in Pairing the device to pair all devices to the same Wiser Hub. |
|
Only one or part of smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). |
|
|
I have only 755WSA smoke alarms without Wiser Hub. |
Identify one
device as Primary and pair all others according to Interconnecting
devices without Wiser Hub. |
|
|
I have 755WSA smoke alarms and standalone 755LPSMA4 / 755RFB2 smoke alarms / RF base but without Wiser Hub. |
Identify one
device as Primary and pair all others 755WSA smoke alarms according
to Interconnecting
devices without Wiser Hub and standalone 755LPSMA4 / 755RFB2
smoke alarms / RF base according to Interconnecting standalone devices. NOTE: If 755LPSMA4 / 755RFB2 is
already installed and paired before, use the Primary unit to pair
with all Wiser smoke alarms.
|
|
|
I have 755WSA smoke alarms and standalone 755LPSMA4 / 755RFB2 smoke alarms / RF base and Wiser Hub. |
All 755WSA smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). NOTE: If 755LPSMA4 / 755RFB2 are already installed
and paired before, reconnect by pairing them again.
|
|
Only one or part of 755WSA smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). NOTE: If 755LPSMA4 / 755RFB2 are already installed
and paired before, reconnect by pairing them again.
|
|