DUG_Iconic Dimmer_Pacific_WSE-00

Pairing the device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.

To pair the device with auto scan:
  1. On the Home page, tap +.
  2. Tap Auto scan > Confirm.
  3. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short-press the push button three times.
    NOTE: Wait for a few seconds until the device search is complete.
    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds for them to be detected.
  6. Tap Next (A), select Iconic Dimmer.
  7. Once the device is added successfully, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?