DUG_Motion_Sensor_Pacific_WSE–00

Sensitivity

Using the Wiser app, you can set the sensitivity of the sensor (such as High, Medium, Low).

To set the sensitivity:

  1. On the Home page, tap All devices > Motion Sensor.
  2. On the device control panel page, tap Settings.
  3. Short press the function key 3 times or simulate the motion to wake up the device.
  4. Tap Sensitivity and select one of the following levels (A):
    • High
    • Medium
    • Low
    NOTE: The high sensitivity level detects the slightest movement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?