0102CT2001

Elegant Form and Intelligent Function

Connected devices
Schneider Home
by Schneider Electric
X Series humidity / motion sensor and fan control
USB A/C receptacle plate

Update your style: fully flush wall plates and premium matte finishes meet IoT-enabled intelligence.

Wi-Fi and Z-Wave connectivity

Intelligent connectivity makes these wiring devices remotely manageable via voice command or app control. With smart wiring devices, create custom lighting scenes, monitor energy use down to the plug level, and much more.





Schneider Home by Schneider Electric

Control switches and outlets remotely and connect to smart devices.













One device, three functions

Save space and time by combining a fan switch, humidity sensor, and occupancy sensor.












Power up, fast

Charge two devices at once faster than average receptacles with high-amperage USB charging.

Power leader with 4.8 ampere total.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?