0600IB1201

Section 3—Performance Tests for Thermal-Magnetic Circuit Breaker

These tests check the performance of thermal-magnetic trip molded case circuit breakers.

General Circuit Breaker Performance Tests

DANGER
Hazard of Electric Shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462.
  • This equipment must be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors and covers before turning on power to this equipment.
  • Do not touch the circuit breaker terminals or the test leads while the circuit breaker is being tested.
Failure to follow these instructions will result in death or serious injury.

Do the performance tests in the order given to maximize the accuracy of the test results.

NOTE: Never do the contact resistance test before doing the instantaneous primary injection testing. The primary injection testing will ensure the contacts are clear of resistive films, oxidation and foreign material.

The following tests are intended to verify that a circuit breaker is operating properly. Precisely controlled factory testing conditions are used to establish the characteristic trip curves. If field test results fall outside the characteristic trip curve tolerance band, carefully evaluate the test conditions and methods for accuracy.

When questionable conditions or results are observed during inspection and performance tests, consult your local field sales office. Circuit breakers with accessories or factory modifications may require special investigation. If it is necessary to return a circuit breaker to the manufacturing facility, use proper packaging and packing materials to avoid shipping damage.

Field Testing Special 500 Vdc Circuit Breakers

Square D UL® Listed 500 Vdc circuit breakers are designed, manufactured and calibrated for use on ungrounded uninterruptable power supplies (UPS). The maximum nominal (loaded) voltage is 500 Vdc and the maximum floating (unloaded) voltage is 600 Vdc.

These circuit breakers are UL Listed when applied with all three poles connected in series as shown on the label of the circuit breaker. The series connection is customer provided and external to the circuit breaker.

Square D UL Listed 500 Vdc circuit breakers are special circuit breakers for dc applications only and must be tested using dc current.

  • Select the correct time-current trip curve. The trip curves show both the thermal and magnetic trip ranges of the circuit breakers.

  • Use a dc power supply to test the circuit breakers as follows:

    Circuit Breaker Time Constant*
    ≤ 400 A dc ≤ 20 ms
    450–2500 A dc ≤ 25 ms
    dc ripple constant ≤ 1% rms.
  • Make sure ambient temperature and circuit breaker temperature is 25°C ± 3 degrees.

  • Remove the circuit breaker from the enclosure. If removing the circuit breaker is not practical, test the circuit breaker in the end-use equipment. If the test results fall outside of the trip curve tolerance, remove the circuit breaker from the enclosure and retest.

  • Use correctly sized cable (per National Electrical Code® [NEC®] tables) with a minimum of four feet (1.22 m) of cable per connection.

  • Connect dc power supply to circuit breaker with all poles connected in series as shown on the circuit breaker label.

  • Make sure connections to circuit breaker are properly torqued.

  • Apply dc test current to trip the circuit breaker. The tripping mechanism in the circuit breaker reacts to the magnetic fields created by the current flowing through the circuit breaker. Apply a dc test current to the circuit breaker of approximately 70% of the expected value. If the circuit breaker does not trip, increase the test current on successive trials until it does trip. When the circuit breaker trips

    1. Reset and close the circuit breaker.

    2. Reapply the dc test current to trip the circuit breaker again.
    3. Record the current and compare to the trip curve.

Field Testing AC Thermal-Magnetic Circuit Breakers

Recommended steps to accurately field test circuit breakers (see test procedures in this manual for specific information):

  • Use correct test equipment.

  • Make sure ambient temperature and circuit breaker temperature is 25°C ± 3 degrees.

  • Remove the circuit breaker from the enclosure. If removing the circuit breaker is not practical, test the circuit breaker in the end-use equipment. If the test results fall outside of the trip curve tolerance, remove the circuit breaker from the enclosure and retest.

  • Use correctly sized cable (per NEC tables) with a minimum of four feet (1.22 m) of cable per connection.

  • Test each pole individually.

  • Make sure connections to circuit breaker are properly torqued.

  • Test circuit breaker and record findings. The tripping mechanisms in the circuit breaker react to the magnetic fields created by the current flowing through the circuit breaker. When current flow is near the trip point of the circuit breaker, the magnetic fields can cause false tripping due to vibration. Do the following steps to minimize the effects of false tripping:

    1. After each current pulse or when circuit breaker trips, reset and turn the circuit breaker on.

    2. Reapply the test current to trip the circuit breaker again.

    3. Record the current and compare to the trip curve.

Performance Tests

Insulation Resistance Test

Severe environmental conditions can reduce the dielectric strength of molded case circuit breakers. Check insulation resistance during electrical system testing.

NOTICE
Hazard of Equipment damage
Do not apply test voltage to control circuits or accessory terminals; damage to electronic and/or low-voltage components can result.
Failure to follow these instructions can result in equipment damage.

To check the insulation resistance, perform the following steps:

  1. De-energize and isolate the circuit breaker.

  2. Clean the circuit breaker as described earlier.

  3. Using a megohmmeter with a capacity of 500–1000 Vdc, apply voltage from:

    1. Each phase-to-ground with the circuit breaker on (circuit breaker contacts closed).

    2. Phase-to-phase with the circuit breaker on (circuit breaker contacts closed).

    3. Between each line and load terminal with the circuit breaker off (circuit breaker contacts open).

  4. Record resistance values. Resistance values of less than one megohm (1,000,000 ohm) should be investigated.

Thermal-Magnetic Circuit Breaker Performance Tests

DANGER
Hazard of Electric Shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462.
  • This equipment must be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Inverse-Time Overcurrent Trip Test

  1. Completely de-energize and remove the circuit breaker from service. Conduct the following tests at 300% of the circuit breaker ampere rating to verify the performance of the thermal tripping element on thermal-magnetic circuit breakers using a high-current, low-voltage ac power supply of less than 24 V.

  2. Test in open air at 25°C (77°F) ambient temperature.

  3. Trip times are measured from a “cold start.” A cold start, as defined by Underwriters Laboratories Inc. Standard 489 occurs at 25°C ± 3° (77°F ± 5°). Therefore, before beginning overcurrent testing, the circuit breaker must be in 25°C (77°F) ambient temperature long enough for all parts to reach that temperature. Circuit breakers that have been in higher ambient temperatures may take two to four hours to reach the steady state temperatures mentioned above.

  4. Connect the circuit breaker to a power supply by using a minimum of four feet (1.2 m) of cable on each connection. Size the cable according to the ampere rating of the tested circuit breaker. Refer to the National Electrical Code Table 310-16; use the 75°C column for proper conductor sizing. Improperly sized cable will affect test results.

  5. Test each pole of the circuit breaker individually at 300% of rated current using a high-current, low-voltage ac power supply.

  6. Record and compare the trip test values to those in Inverse-Time Overcurrent Trip Test. As long as the recorded trip times are below the maximum trip times, the circuit breaker is providing acceptable thermal protection.

If verification of the manufacturer’s data is required, compare the trip times to the 300% trip range shown on the trip curve for the specific circuit breaker. If field test results fall outside the characteristic trip curve tolerance band, the test conditions and methods should be carefully evaluated for accuracy. A small error in test current results in a large error in trip time.

Inverse-Time Overcurrent Trip Test*

Rated Continuous Current Maximum Trip Time
240 V 480 V / 600V
0–30 A 60 sec.  
31–50 A 80 sec. 100 sec.
51–100 A 140 sec. 160 sec.
101–150 A 200 sec. 250 sec.
151–225 A 230 sec. 275 sec.
226–400 A 300 sec. 350 sec.
401–600 A   450 sec.
601–800 A   500 sec.
801–1000 A   600 sec.
1001–1200 A   700 sec.
1201–1600 A   775 sec.
1601–2000 A   800 sec.
2001–2500 A   850 sec.
2501–5000 A   900 sec.

Instantaneous (Magnetic) Trip Test

This test simulates short-circuit conditions using a low-voltage test supply. To keep stray magnetic fields from affecting test results, test cables exiting the circuit breaker must be parallel with the current path of the circuit breaker for a minimum of 10 in (254 mm). Test results can also be influenced by the wave shape of the supply current. Use a power source with true sinusoidal output and a true RMS or analog ammeter to ensure accurate results. To verify the performance of the instantaneous (magnetic) trip element, proceed as follows:

NOTE: Test PA and PH circuit breakers with the circuit breaker mounted on a terminal pad kit (catalog number PALTB). PC circuit breakers should be tested with the circuit breaker mounted on the terminal pad kit provided with the circuit breaker.

Test NA and NC circuit breakers in the end-use equipment or lying flat on a piece of 1/8 in. (3 mm) thick steel.

  1. Set the circuit breaker instantaneous (magnetic) trip adjustment, if provided, to the high setting. Tests conducted at the high setting ensure instantaneous trip protection exists at all lower settings.

  2. Connect the circuit breaker to the low-voltage test source with any convenient length of conductor.

  3. Test each pole individually by the pulse method as follows:

    The pulse method requires that the test equipment have a controlled closing and a pointer-stop ammeter, a calibrated image-retaining oscilloscope, or a high-speed, sampling-rate digital ammeter. The pulse method involves the following steps:

    1. Connect one pole of the test circuit breaker to the test equipment.

    2. Set the current control of the test equipment to a value approximately 70% of the instantaneous trip current setting.

      Example: If the instantaneous (magnetic) trip setting is 2000 A, set the test equipment to 1400 A.

    3. After the circuit breaker is properly connected and adjusted, apply current in approximately 10-cycle pulses.

    4. Starting at 70% of the instantaneous trip setting, increase the current of each pulse until the circuit breaker trips. After each pulse, move the circuit breaker handle to the full reset position and then to the on position.

    5. Repeat step D to recheck and verify this value. Start with the current level below the value measured in step D to ensure a “no trip” on the initial pulse.

  4. Record current level and trip time. To ensure protection of the rated conductor, the current necessary to trip the circuit breaker instantaneously must not exceed 140% of the high setting for circuit breakers 250 A frame size and below, and 125% of the high setting for circuit breakers 400 A frame size and above. These settings are printed on the faceplate label of the circuit breaker. If currents higher than these maximum levels are necessary to trip the circuit breaker, consult your local field sales office.

If field test results fall outside the characteristic trip curve tolerance band, the test conditions and methods must be carefully evaluated for accuracy.

Rated Current Hold-In Test

This test should be performed only on circuit breakers that have been nuisance tripping under normal conditions.

Conduct the test in a 25°C (77°F) ambient temperature using a high-current, low-voltage ac power supply. Follow the same procedure used in the Inverse-time Overcurrent Trip Test, through . Connect all poles of the circuit breaker in series using cables with the appropriate ampacity for the application. These cables should be 4 ft. (1.22 m) long per terminal (8 ft. [2.43 m] total between poles). All connectors must be properly torqued according to the circuit breaker label specifications.

The circuit breaker should not trip when 100% of the device’s rated current is applied for one hour for circuit breakers rated less than 100 A, or two hours for circuit breakers rated more than 100 A. If the circuit breaker trips, reset and move the handle from the off to on position several times while under load, then repeat the test. If the tripping condition continues, contact your local field sales office.

Contact Resistance Test

Circuit breaker pole resistance tests are not reliable indicators of circuit breaker performance because the resistance values are influenced by a number of transient factors including contact surface oxidation, foreign material between the contacts, and testing methods. NEMA AB 4 paragraph 6.4.1 states: “The millivolt drop of a circuit breaker pole can vary significantly due to inherent variability in the extreme low resistance of the electrical contacts and connectors. Such variations do not necessarily predict unacceptable performance and shall not be used as the sole criteria for determination of acceptability.”

High pole resistance may also be caused by eroded contacts, low contact force, and loose termination. The only one of these factors likely to be present on a new circuit breaker is a loose termination, since the contacts are new and there has been no opportunity for contact pressure to have drifted from the factory setting. A loose termination can be corrected in the field.

If a contact resistance test is done, it is important to do it after the contacts have been conditioned by instantaneous primary injection testing to ensure the contacts are clear of resistive films, oxidation and foreign material. If the circuit breaker has been in service with no performance issues, (overheating or nuisance tripping), contact resistance measurements are redundant and of little value.

Square D recommends that a DLRO (Digital Low Resistance Ohmmeter) be used, using a 10 A dc test current for circuit breaker ratings below 100 A, and using 100 A dc for circuit breakers rated 100 A and above. the median (middle) value of three readings (toggling the circuit breaker between each reading) should be recorded for each pole tested. If this value is equal to or less than the value listed in Maximum Micro-Ohms Per Pole, the pole is acceptable. If the reading is higher, the cause should be investigated and corrected if possible. Contact your local field office for more information.

Maximum Micro-Ohms Per Pole

Circuit Breaker Micro-Ohms (u ohm) Circuit Breaker Micro-Ohms (u ohm) Circuit Breaker Micro-Ohms (u ohm) Circuit Breaker Micro-Ohms (u ohm)
Type Rating Type Rating Type Rating Type Rating
FA, FH, FC 15 38,400 KA, KH 70 3,420 MA, MH 125 1,970 LD, LG, LJ, LL, LR 250 630
20 23,100 80 2,620 175 1,120 400 240
25 14,800 90 2,390 200 890 600 160
30 10,400 100 1,930 225 730 NSF, CG, CJ 16 35,000
35 7,860 110 1,620 250 600 25 14,000
40 6,010 125 1,250 300 425 32 7,000
45 5,180 150 890 350 322 40 6,000
50 4,190 175 680 400 246 50 4,000
60 2,910 200 540 500 180 63 2,800
70 2,340 225 430 600 140 80 1,700
80 1,790 250 350 700 115 100 1,100
90 1,430 KC, KI 110 1,620 800 96 NSJ 400 240
100 1,160 125 1,250 900 83 600 140
FD, FG, FJ 15 34,700 150 890 1000 67 MG, MJ 300 780
20 19,500 175 680 HD, HG, HJ, HL, HR 15 35,000 350 570
25 12,500 200 540 20 23,000 400 440
30 9,550 225 430 25 14,000 450 350
35 7,020 250 350 30 10,400 500 280
40 6,800 LA, LH 125 1,500 35 7,860 600 190
45 5,780 150 1,200 40 6,010 700 140
50 5,000 175 980 45 5,180 800 110
60 4,120 200 770 50 4,190 NA, NC 600 138
70 3,510 225 610 60 2,910 700 131
80 3,170 250 510 70 2,340 800 105
90 2,510 300 480 80 1,790 900 100
100 2,260 350 330 90 1,430 1000 82
110 2,060 400 310 100 1,200 1200 69
125 1,800 LI, LC 300 589 110 1,160 PA, PH, PC 600 132
FI 20 26,200 350 513 125 1,100 700 123
25 17,700 400 308 150 1,020 800 100
30 12,300 450 310 JD, JG, JJ, JL, JR 150 890 1000 77
35 9,070 500 286 175 680 1200 66
40 7,330 600 209 200 600 1400 61
45 5,790       225 525 1600 50
50 4,930       250 450 1800 43
60 3,420             2000 38
70 3,020             2500 33
80 2,310             NSF, CG, CJ 16 35,000
90 1,980              
100 1,600            

Remove Test Connections

Upon completing testing:

  • Remove test connections from circuit breaker.

  • Inspect connections for damage caused by testing.

Additional Information

For more information concerning Square D circuit breakers, refer to the appropriate instruction manual. These manuals contain installation instructions, mounting information, safety features, wiring diagrams, and troubleshooting charts for specific circuit breakers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?