0611DB1205

Section 3— Circuit Breaker Communication Network Options

All PowerPacT H-, J-, and L-frame circuit breakers devices can be equipped with the communication function using a pre-wired connection system and a Modbus communication interface module. The interface module can be connected directly or through the front display module (FDM121).

The PowerPacT H-, J-, and L-frame circuit breakers can be integrated in a Modbus communication network. Four functional levels can be used separately or combined to adapt to all supervision requirements.

Level

Function

Communication of status indications

Compatible with PowerPacT H-, J-, and L-frame circuit breakers and automatic switches. Use the BSCM module to access the following information:

  • ON/OFF position

  • trip indication

  • fault-trip indication

Communication of commands

Available on all circuit breakers and automatic switches with communicating motor operators, the remote control can be used to:

  • open

  • closed

  • reset

Communication of measurements with MicroLogic 5 / 6 A or E trip unit

This level provides access to:

  • instantaneous and demand values

  • maximums/minimums

  • energy metering

  • demand current and power

  • power quality

Communication of operating assistance with MicroLogic 5 / 6 A or E trip unit

This level also provides access to:

  • protection and alarm settings

  • time-stamped histories and event tables

  • maintenance indicators

PowerPacT H-, J-, or L-frame circuit breaker is connected to the Modbus communication interface module (IFM) or front display module (FDM121) through the internal terminal block for the NSX cord.

The front display module is connected to the Modbus communication interface module by a communication cable with RJ45 connectors on both ends.

  1. Modbus network

  2. Modbus communication interface module

  3. NSX cord

  4. Internal terminal block for communication using the NSX cord

  5. BSCM module

  6. Prefabricated wiring

  7. MicroLogic trip unit

  8. FDM121 display

  9. RJ45 cable

  10. Line terminator (for unused connectors, if applicable)

Circuit Breaker Communication

PowerPacT™ H-, J, and L-frame circuit breakers with MicroLogic™ trip units can be integrated into a communication network created using Modbus™ protocol. Use data transmitted by the communication network to provide supervision and monitoring for an installation.

This communication network offers the options of:

  • Reading remotely:

    • The circuit breaker status

    • Measurements

    • Operating assistance information

  • Controlling the circuit breaker remotely

For more information about the Modbus communication network, refer to the specific circuit breaker user manual.

For more information about the communication network, refer to the MasterPacT and PowerPacT UL/ANSI ULP System — Installation and User Guide.

Remote readout of the circuit breaker status is accessible by all circuit breakers equipped with a BSCM. The following data is available using the communication network:

  • Open/closed position (OF)

  • Trip indicator (SD)

  • Electrical fault indicator (SDE)

For more information, refer to the bulletin shipped with the circuit breaker.

Access the measurement readout with MicroLogic 5 and 6 trip units. For more information about measurements, refer to the EPC Online Help.

Access the operating assistance readout with MicroLogic 5 and 6 trip units. The following operating assistance information is available:

The circuit breaker remote control is accessible by any circuit breaker with a MicroLogic trip unit, a BSCM, and a communicating motor mechanism. The following commands are available using the communication network:

  • Circuit breaker opening

  • Circuit breaker closing

  • Circuit breaker reset

For more information, refer to the bulletin shipped with the circuit breaker.

Maintenance Indicators

BSCM Counters

The counters embedded in the BSCM generate information relating to the number of volt-free contact operations. These volt-free contacts qualify:

  • The number of open/close operations (OF contact) and open on fault operations (SD and SDE contacts) on the PowerPacT H-, J-, or L-frame circuit breaker

  • The number of close, open, and reset operations on the motor mechanism

Access the maintenance counters embedded in the MicroLogic trip unit with the communication option.

  • Counters are assigned to each type of protection:

    • Long time protection

    • Short-time protection

    • Ground-fault protection

    • Jam motor protection

    • Phase unbalance protection

    • Long start motor protection

    • Underload motor protection

  • Ten counters are assigned to the alarms associated with measurements. These counters reset if the alarm is reconfigured.

  • One counter indicates the number of operating hours. This counter is updated every 24 hours.

  • Four counters are assigned to the load profile: Each counts the number of operating hours per loading section (for example, one counter indicates the number of operating hours for the loading section 50–79% of In. Six counters are assigned to the temperature section (for example, one counter indicates the number of operating hours for the temperature section 140–165°F (60–74°C).

  • Use maintenance counters to enter quantitative information about operations performed on the MicroLogic trip unit (such as the number of push to trip tests) or the status of the MicroLogic trip units (such as the number of Err screens or protection setting lock/unlock operations).

  • One counter indicates the amount of wear on the circuit breaker contacts as a percentage. When this figure reaches 100%, the contacts must be changed.

History and Time-Stamped Information

History

MicroLogic trip units generate three types of history:

  • History of alarms associated with measurements (the last ten alarms are recorded)

  • History of trips (the last 18 trips are recorded)

  • History of maintenance operations (the last ten operations are recorded)

Time-Stamped Information

Time-stamped information displays dates for important information such as previous protection settings and minimum/maximum current, voltage, and network frequency values.

The table of time-stamped information describes:

  • The previous protection configurations and corresponding dates

  • The minimum and maximum voltage measurement values and corresponding dates

  • The maximum current measurement values and corresponding dates

  • The minimum and maximum network frequencies and corresponding dates

The time when the minimum and maximum values were reset is also available.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.