Section 5 — EcoStruxure Power Commission (EPC) Software
Function Setting
EcoStruxure Power Commission (EPC) Software works with MicroLogic trip units to:
-
Check and configure
-
Metering functions
-
Alarms
-
Assignment of the SDx Module outputs
-
BSCM functions
-
ModbusTMInterface Module
-
-
Modify passwords
-
Save configurations
-
Edit configurations
-
Download the firmware
Some functionality may require the inclusion of a test kit(s) found in Section 7 of The Digest (Reference 0100CT1901).

Using the EPC Software
WARNING |
|---|
|
potential compromise of system availability, integrity,
and confidentiality
Change default passwords at first use to help prevent
unauthorized access to device settings, controls and information.
Disable unused ports/services and default accounts to
help minimize pathways for malicious attackers.
Place networked devices behind multiple layers of cyber
defenses (such as firewalls, network segmentation, and network intrusion
detection and protection.
Use cybersecurity best practices (for example, least privilege,
separation of duties) to help prevent unauthorized exposure, loss,
modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The EPC software can be used:
-
In standalone mode, directly on the MicroLogic trip unit and SI kit connected to the test port and to a PC over USB.
-
Using the communication network
For more details, see the EPC Software Online Help under the Help menu in EPC.
Use offline mode to configure the protection, metering, and alarm functions of the MicroLogic trip unit in the EPC software.
For more details on offline mode, see the EPC Software Online Help.
WARNING