0613CT0001

Accessory Dimensional Drawings

Accessory Dimensions

IFE Ethernet Interface

 
   

IO (Input/Output) Application Module

 
   

IFM Modbus-SL Interface

 
   

FDM121 Switchboard Display Dimensions

 
   

FDM121 Switchboard Display Mounting Through Panel

 
   

FDM121 Switchboard Display Mounting On Panel

 
 

FDM128 Switchboard Display Dimensions

 
   

FDM128 Switchboard Display Mounting on Panel

 
   
 

MasterPact NT and NW Circuit Breaker Communication

A FDM121 (TRV00121)   E IO module (LV434063)   I ULP termination (TRV00880)   M NSX cord
B IFE module master (LV434011   F MasterPact NT/NW circuit breaker   J FDM128 (LV434128)      
C IFE module (LV434010)   G PowerPact P/R circuit breaker   K ULP cable      
D IFM module (TRV00210)   H PowerPact H/J/L circuit breaker   L Circuit breaker ULP cord      

Fixed MasterPact NT and NW Connection to the Communication Interface Module

Drawout MasterPact NT and NW Connection to the IO and Communication Interface Module

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?