Installing the Deadfront Assembly for a Sub-Feed Circuit Breaker onto an NF Panelboard
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
-
Remove the line and load end deadfront covers from the deadfront assembly. Discard the 10-32 x 7/16-in. mounting screws and deadfront covers.
-
Install the line end deadfront cover using the two 10-32 x 7/16-in. mounting screws supplied in the kit.
NOTE: Place the line end deadfront cover and the branch circuit breaker cover based on the top feed or bottom feed orientation. -
Assemble the circuit breaker deadfront cover to the deadfront extension supplied in the kit and install onto the deadfront assembly using the new 10-32 x 7/16-in. mounting screws, also supplied in the kit. Install the circuit breaker escutcheon by pressing it against the circuit breaker deadfront cover and snap it into place.
DANGER