Installing the N600MPPL kit, for a PowerPacT L Main Circuit Breaker, onto an NF Interior
Tools Needed
-
#2 square-head Robertson® driver
-
Torque wrench with 3/8-in. Allen® driver
-
Torque wrench with 5/32-in. Allen driver
-
Flat-head screwdriver
-
Phillips® #2 screwdriver
-
4 mm Allen driver
-
6 mm Allen driver
-
8 mm Allen driver
-
Torque wrench with 16 mm hex head nut driver
Installation
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
hazard of equipment damage
Failure to follow these instructions can result in equipment damage.
|
-
Remove the backplane insulator from the 600 A panelboard by unsnapping the four corners from the end supports, and discard.
NOTE: 600 A panelboard interiors are required for 400 A applications. -
Remove the deadfront assembly. Retain the four screws for reuse.
-
Remove the line lugs, their screws, and lug vertical barriers from the panelboard bus, and discard.
NOTE: Leave the neutral lugs in place.NOTE: Slide the lug barriers up to remove them from the NF end cap.
DANGER