Table 88

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 88

Motor FLC (A)

Thermal Unit Number

0.39–0.40

A.49

0.41–0.44

A.54

0.45–0.49

A.59

0.50–0.57

A.65

0.58–0.61

A.71

0.62–0.66

A.78

0.67–0.73

A.86

0.74–0.80

A.95

0.81–0.90

A1.02

0.91–0.97

A1.16

0.98–1.09

A1.25

1.10–1.23

A1.39

1.24–1.57

A1.86

1.58–1.66

A1.99

1.67–1.79

A2.15

1.80–1.99

A2.31

2.00–2.31

A2.57

2.32–2.50

A2.81

2.51–2.66

A3.61

2.67–2.85

A3.95

2.86–3.26

A4.32

3.27–3.49

A4.79

3.50–3.92

A5.30

3.93–4.20

A5.78

4.21–4.49

A6.20

4.50–4.64

A6.99

4.65–4.94

A7.65

4.95–5.62

A8.38

5.63–6.39

A9.25

6.40–6.82

A9.85

6.83–7.27

A11.0

7.28–7.71

A11.9

7.72–8.13

A13.2

8.14–8.64

A14.1

8.65–9.15

A14.8

9.16–9.97

A16.2

9.98–11.0

A17.9

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?