9065CT9701R03/21

Mounting the Thermal Units

Example of Thermal Unit Type Designation on front of Starter

Always be certain the correct thermal units are installed in the starter before operating the motor. Thermal units should always be mounted so that their type designation can be viewed from the front of the starter as shown in the figure Example of Thermal Unit Type Designation on front of Starter. Melting alloy thermal units should be mounted so that the tooth of the pawl assembly can engage the teeth of the ratchet wheel when the reset button is pushed.

Mounting surfaces of starter and thermal units should be clean and care should be taken to insure that thermal unit mounting screws are fastened securely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.