Assign Model Names and Autoupdaters

Assign the following model names and autoupdaters. Model names are listed after the feature class.

The UFMVISIBLE model name determines which layers are visible when the user is viewing the manhole diagrams (i.e., precision drawing mode). Only layers with the UFMVISIBLE model name assigned will be displayed. You may wish to display other layers (e.g., conductor) while viewing underground diagrams. Assign this model name to these layers.


Cables (Primary, Secondary, Fiber): UFMVISIBLE


Conduit: UFMVISIBLE

Special Autoupdaters

Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.

Feature Property

Autoupdater

On Feature Update

ArcFM UFM Conduit Cross Section


Duct: UFMDUCT, UFMVISIBLE

Field Model Names

Field

Field Model Name

PhaseDesignation

PHASEDESIGNATION

DuctPosition

DUCTID

DuctName

DUCTNAME

Available

DUCTAVAILABILITY

Occupied

DUCTOCCUPIED

DuctSize

DUCTSIZE

Material

DUCTMATERIAL

HasSubducts

HASSUBDUCTS

Special Autoupdaters

Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.

Feature Property

Autoupdater

On Feature Create

ArcFM UFM Duct to Conduit Synch

On Feature Update

ArcFM UFM Duct to Conduit Synch, ArcFM UFM Resize Duct AU, ArcFM UFM Update Opposite Duct Attributes

On Feature Delete

ArcFM UFM Duct to Conduit Synch, ArcFM UFM Delete Duct Connector


DuctAnnotation: UFMANNOTATION, UFMVISIBLE


DuctBank: UFMDUCTBANK, UFMVISIBLE

Field Model Names

Field

Field Model Name

FacilityID

FACILITYID


DuctBankAnchor: UFMDUCTBANKANCHOR, UFMVISIBLE

Field Model Names

Field

Field Model Name

SymbolRotation

SYMBOLROTATION

Split Information

Set this property on the Object Info tab of the ArcFM Properties Manager.

Feature Property

Value

Split On Edit

No

The DuctBankAnchor feature class is only used when Conduit Manager creates a composite favorite. These features are never placed by the user. The Split On Edit property is set to No to prevent the potential for inadvertantly splitting a line feature. 


DuctConnector: UFMDUCTCONNECTOR, UFMVISIBLE

Field Model Names

Field

Field Model Name

PhaseDesignation

PHASEDESIGNATION


DuctDefinition: DUCT

Field Model Names

Field

Field Model Name

DuctSize

DUCTSIZE


DuctNoteAnno: UFMANNOTATION, UFMVISIBLE


Splice: UFMSPLICE


UFMAnchor: UFMANCHOR, UFMVISIBLE

Field Model Names

Field

Field Model Name

SymbolRotation

SYMBOLROTATION

Split Information

Set this property on the Object Info tab of the ArcFM Properties Manager.

Feature Property

Value

Split On Edit

No

The UFMAnchor feature class is only used when Conduit Manager creates a composite favorite. These features are never placed by the user. The Split On Edit property is set to No to prevent the potential for inadvertantly splitting a line feature. 


UFMFloor: UFMFLOOR, UFMVISIBLE

Field Model Names

Field

Field Model Name

FacilityID

FACILITYID


UFMInsetFrameSource: INSETFRAMESOURCE, UFMINSETFRAMESOURCE

IMPORTANT: The UFMINSETFRAMESOURCE model name may be assigned to only one feature class. Errors will occur if it is assigned to multiple layers.

Field Model Names

Field

Field Model Name

Title

INSETFRAMETITLE


UFMWall: UFMVISIBLE, UFMWALL

Field Model Names

Field

Field Model Name

FacilityID

FACILITYID

UFMWall features must snap to the UFMFloor features. Use the ArcFM Snapping Manager to set this.


UFMWallDimensioning: UFMDIMENSION, UFMVISIBLE


UndergroundStructure: MANHOLEFEATURESNAP, STRUCTURE

Field Model Names

Field Name

Data Type

FacilityID

FACILITYID

SymbolRotation

SYMBOLROTATION

FacilityDiagram

FACILITYDIAGRAM

Special Autoupdaters

Assign these autoupdaters on the Object Info tab of the ArcFM Properties Manager.

Feature Property

Autoupdater

On Feature Update

ArcFM Populate Facility ID


Conduit_Cable relationship: (primary, secondary, fiber optic)

The autoupdater assigned below calls the ArcFM UFM Conduit to Conductor Relationship AU and the ArcFM Manage Conduit Manager Relationship Changes AU. It should replace the ArcFM Manage Conduit Manager Relationship Changes AU assigned during the basic Conduit Manager configuration.

Relationship Autoupdaters

Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager.

Feature Property

Autoupdater

On Relationship Created

ArcFM Conduit to Conductor Composite

On Relationship Updated

ArcFM Conduit to Conductor Composite

On Relationship Deleted

ArcFM Conduit to Conductor Composite


ConduitSystem_DuctBank relationship:

Relationship Autoupdaters

Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager.

Feature Property

Autoupdater

On Relationship Created

ArcFM UFM Populate Conduit Blob on Duct Bank Relationship Creation AU


Cable_Duct relationships: (primary, secondary, fiber)

Relationship Autoupdaters

Assign these autoupdaters on the Relationship Class Options tab of the ArcFM Properties Manager. These should be assigned to all Cable_Duct relationships (e.g., PriUGElectricLineSegment_Duct, SecUGElectricLineSegment_Duct, FiberCable_Duct).

Feature Property

Autoupdater

On Relationship Created

ArcFM UFM Duct to Conductor Relationship

On Relationship Updated

ArcFM UFM Duct to Conductor Relationship

On Relationship Deleted

ArcFM UFM Duct to Conductor Relationship

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?