Configure Duct Size Options
To allow the ability to place ducts within ducts in your geodatabase, follow these steps:
- Add the following field model names to the Electric Field
Model Name domain. If you are using the sample data, this field model
name may already exist in that domain.
DUCTSIZE
ACTUALDUCTSIZE
- Add the following fields to the DuctDefinition object class.
Field Name
Data Type
Domain
DuctSize
text, float, or double
ULS Size
ActualSize
text, float, or double
ULS Size Actual
- Assign the following model names.
DuctDefinition object class
Field
Field Model Name
Custom Field Editor
DuctSize
DUCTSIZE
ArcFM Duct Size Editor
ActualSize*
ACTUALDUCTSIZE
* NOTE: The ActualSize field allows the user to store the actual size of the duct and place a duct of relative size on the map. This field is not required to place ducts within ducts.
- When placing a duct within a duct, the user must choose
a duct that is smaller than the master duct. To restrict the duct
size the user can choose to place within the master duct, assign the
ArcFM Duct Size field editor to the DuctSize field (field with the
DUCTSIZE field model name) on the Duct Definition object class. Field
editors may be assigned on the Field Info tab in the ArcFM Properties
Manager.NOTE: When the ACTUALDUCTSIZE field model name is present, Conduit Manager tracing ignores the DuctSize field and instead calculates sizes based on the value in the field to which the ACTUALDUCTSIZE field model name is assigned.