Fiber Circuit Type

TIP: This domain is not required but can be used to designate types of circuits, e.g., if it’s dark fiber or used for DWDM (dense wavelength division multiplexing).

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

1G Ethernet

1G Ethernet

10G Ethernet

10G Ethernet

10M Ethernet

10M Ethernet

CWDM

CWDM

Dark Fiber

Dark Fiber

DWDM

DWDM

OC3

OC3

OC12

OC12

OC48

OC48

OC192

OC192

Other

Other

Unknown

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?