Fiber Passive Device Type

Passive devices are those that are not powered, while active devices are those that are powered. Those two concepts are important in the world of WDM (wavelength division multiplexing).

TIP: This domain is not required, and the values provided are just examples. If you include this domain, the coded values should contain items from your inventory.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Attenuator

Attenuator

Dispersion Compensator

Dispersion Compensator

Mux

Mux

RF Splitter

RF Splitter

Splitter

Splitter

Terminator

Terminator

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?