SCADA Service Configuration
- Change the log file location, if required. By default the
log file will be placed in C:\Responder\Logs.
<file value="C:\Responder\Logs\SE.Responder.Integration.ScadaService.log"/>
- Change the MSMQ ComputerName to the FQDN of the Responder
Message Router Server.
Verify that the “ComputerName” is not populated, it should say “ComputerName”:
<wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem" />
Set the “ComputerName” here:
<channel type="Miner.Responder.Shared.Channels.MSMQ.MSMQChannel, Miner.Responder.Shared" ComputerName="ComputerName " responseTimeout="00:00:03" />
- The following configurations are made in the Miner.Responder.RxIF.ScadaService.exe
XML configuration file, which by default is found in directory C:\Program
Files (x86)\Miner and Miner\Responder\Integration\Scada Service:
Config Key
Config Description
Default Config Value
ScadaIncidentRemarks
Remarks on Incidents created as a result of SCADA device operation
Created by SCADA
Scada.MomentaryRemarks
Remarks on Incidents created as a result of device operation of SCADA devices for momentary outages
Auto Reclose occurred between {0} and {1}
ProcessWaitInterval
Time between two subsequent processing cycles for analyzing the SCADA events.
0:00:15
Scada.ProcessMomentaryWaitInterval
Time between two subsequent processing cycles for operating the devices in Responder.
0:00:15
Scada.OptimizeScadaIncidentCreation
Flag to use optimized mechanism of Incident creation/device operation.
IMPORTANT: Switching this configuration to TRUE significantly enhances the performance of SCADA incident creation. However, this bypasses Responder code that considers incidents submitted before the SCADA incident, but within a configured time threshold, from being rolled up into SCADA incidents. The threshold defaults to 20 seconds. See Modify Time Threshold for details how adjust the default. This threshold is primarily needed if communication between integrations causes AMI events triggered by a SCADA device going out to reach Responder before the SCADA event that caused that outage in the first place. Otherwise, it is generally safe for SCADA events to not consider pre-existing incidents, calls, and events for roll up.FALSE
Scada.NumberOfRetryAttempts
Number of tries to operate the device before moving to the new Scada Device operation
0
ScadaClassModelName
Class model name to be assigned to identify the SCADA device in the geodatabase.
SCADAFEATURECLASS
ScadaFieldModelName
Field model name to identify the Scada Device using the Field assigned this model name.
SCADADEVICEID
LogMomentaryOutages
Flag to control the incident creation for the momentary outages.
TRUE
CallRemarks
Remarks on Incidents created by IVR.
Call by IVR.
StaleEventThreshold
EVENTTIME timestamp in HTTP endpoint data received over this threshold compared to system time are not processed and are errored out back to the source system.
02:00
MomentaryEventThreshold
Time between PowerDown and PowerUp events that are within this threshold are considered momentary.
IMPORTANT: If the RECIEVETIME of the event at the HTTP endpoint is greater than the PowerUp EVENTTIME, the event is not treated as momentary.00:01:00
FilterDuplicates
Multiple incidents will not be created when SCADA events are created for the same device.
TRUE
Scada.AllowDelayProcessing
Flag that controls the behavior of device operations and introduces a delay defined by
Scada.AllowedTimeToProcessDevice
.FALSE
Scada.NumberOfRetryAttempts
Number of times to retry before ignoring the device operation.
0