Web Configuration for AMI Using Multispeak (optional module)

The table below shows web.config settings used for optional integration with Multispeak.

Config Key

Config Description

Config Value

Ami.StaleEventThreshold

Events received after this threshold compared to the system time are considered stale and not processed.

02:00:00

Ami.MomentaryEventThreshold

Time between PowerDown and PowerUp events that are within this threshold are considered momentary.

00:01:00

Ami.EventMap

Mapping of AMI Events defined in Multispeak and required in Responder.

NOTE: This setting appears only in Multispeak 3.0AB configuration. It is not included in Multispeak 4.1.6.

Ami.DefaultEventMap

Ami.CDEventMap

Mapping of AMI Events defined in Multispeak for Remote Connect and Disconnect events and its required values in Responder.

Ami.DefaultCDEventMap

Ami.RequireDayLightAdjustment

Set this flag if adjustment is required due to Daylight Saving Time.

FALSE

Ami.DayLightOffsetMins

Configure the time adjustment required when Daylight Savings Time is in effect.

60

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?