Configure Trace Tools
Before using ArcFM Trace Tools in ArcFM Viewer they must be configured according to the instructions provided in the Configuring ArcFM Solution topic in the Desktop Configuration Guide. In addition to the standard configuration ArcFM Viewer requires an additional model name.
The following model names must be assigned to all network edge feature classes that may participate in an ArcFM trace.
Feature Class |
Model Name |
---|---|
All Electric Network Edge feature classes that participate in electric tracing |
ELECTRICNETWORKEDGE |
All Gas Network Edge feature classes that participate in gas tracing |
GASNETWORKEDGE |
All Water Network Edge feature classes that participate in water tracing |
WATERNETWORKEDGE |
Refer to the assign model names topic in ArcCatalog Tools for information about assigning them to feature classes.