Manually Converting Workspace Packets

To convert workspace packets to XML packets, follow the steps below.

  1. In the Process Framework Administration tool, create a task and assign it the Convert to XML Packet subtask. 
  2. Send all existing sessions and designs to the Enterprise. If any sessions or designs are left in a directory folder, they cannot be converted.
  3. Open Workflow or Session Manager.
  4. Select the design or session you want to convert.
  5. Go to the Task tool. Choose the conversion task you created from the menu, and click the Execute Task button.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?