Circuits
When you locate a circuit, Wavepoint provides two tabs: Details and Path.
Details
This tab shows the circuit’s start and end points, as well as other high-level attributes.
Path
This tab displays a one-line subway diagram of the circuit. The following symbols help you orient yourself within the diagram:
|
Symbol |
Description |
|---|---|
|
The start of the circuit |
|
|
The origin of the trace |
|
|
The end of the circuit |
|
|
A patch location |
|
|
A splice |
The diagram also shows ports through which the circuit passes, fibers and their glass lengths, as well as trays at splice cases.

The Circuit Path diagram contains additional information and navigation tools: