Using Overview
Wavepoint delivers your fiber network data via a lightweight web application. Use it to locate, view, and trace features in your network, as well as inspect connectivity and network design.
One of the most helpful features of Wavepoint is the use of static URLs. When you navigate to a cable, splice, patch location, circuit, etc., that feature’s URL is static and remains the same in perpetuity. This means you can copy and paste that URL, share it with others at your company, and they are only one click away from navigating to the feature in question. This also opens up possibilities to include the URL in GIS maps, reports, work orders, and more.
Before you Search, locate on the Map, or Trace fiber facilities, it is a good idea to ensure all the desired layers are visible on the map. After launching the application, next to the Search field, click the Layers drop-down:
If a layer you expected is not present, see the help topic Publish a Map Service with Fiber Data in the Configuration Guide.