Multispeak (optional module)
-
RxIF.Multispeak30ab_####_Release.msi
-
RxIF.Multispeak416Service_####_Release.msi
The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.Multispeak30ab_1061b_Release.msi, and the 10.8.1 installer name is RxIF.Multispeak30ab_1081_Release.msi.
- Run the appropriate Multispeak MSI installer. In the Welcome dialog, click Next.
- Change the Application Pool to SE.Responder.Integration, then click Next.
- Choose a database and click Next.
- Type the credentials for the database and click Next.
- If Responder Web is installed, the same install location will be used. Otherwise ensure that the location is set to the IIS web root, e.g., C:\inetpub\wwwroot\ or use the Browse button to select it, and click Next.
- Start the installation by clicking Install.
- The installation will complete and the files will be deployed
in C:\inetpub\wwwroot\SE.Responder.Integration.Multispeak30ab and C:\inetpub\wwwroot\SE.Responder.Integration.Multispeak416.Service respectively.Repeat the above steps for Multispeak 4.1.6.