Web Configuration for SCADA (optional module)
|
Config Key |
Config Description |
Config Value |
|---|---|---|
|
Scada.EventMap |
Mapping of SCADA Events defined in Multispeak and required in Responder |
Scada.EventMap |
|
Scada.RequireDayLightAdjustment |
Set this flag if adjustment is required due to Daylight Saving Time. |
TRUE |
|
Scada.DayLightOffsetMins |
Configure the time adjustment required when Daylight Savings Time is in effect. |
60 |
|
StaleEventThreshold |
EVENTTIME timestamp in HTTP endpoint data received over this threshold compared to system time are not processed and are errored out back to the source system. |
02:00:00 |
|
MomentaryEventThreshold |
Time between Open and Close events that are within this threshold are considered momentary. |
00:01:00 |
|
ScadaIncidentRemarks |
Remarks on incidents created by SCADA. |
Created by SCADA. |
|
FilterDuplicates |
Multiple incidents will not be created when SCADA events are created for the same device. |
TRUE |
|
ScadaClassModelName |
Class model name to be assigned to identify the SCADA device in the geodatabase. |
SCADAFEATURECLASS |
|
ScadaFieldModelName |
Field model name to identify the SCADA Device using the Field assigned this model name. |
SCADADEVICEID |
|
IsRegistrationRequired |
Configuration flag to determine if the headend AMI system needs an OMS system to request a subscription to receive meter event notifications. |
FALSE |
|
AlwaysUnsubscribeAndThenSubscribe |
Configuration flag to determine if the AMI headend system is expecting the OMS System to unsubscribe the existing subscription before requesting a new subscription or subscribe regardless of the previous one. |
FALSE |