BQT43203

Product Related Information

Read and understand the following precautions before performing any procedures in this guide.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn OFF all power supplying this equipment before working on or inside equipment, or if energized work is necessary, follow all OSHA and NFPA 70E safe work practices for energized electrical equipment work.
  • Always use properly rated voltage sensing device to confirm the electrical state of equipment.
  • All unused spaces must be filled with IP2X blank fillers and blank extensions.
  • Replace all devices, doors and covers after completion of work.
Failure to follow these instructions will result in death or serious injury.

WARNING: This product can expose you to chemicals including Nickel compounds, which are known to the State of California to cause cancer and Bisphenol A (BPA), which is known to the state of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?