BQT43203

Kit Contents

Kit Content

Catalog Number

Description

Application

ILSSKIP2X

1.5 in. Shutters kit IP2X I-Line

Quantity 4

Panelboard

ILBMSIP2X

Refer to ILBMSIP2X — Kit Contents

ILBMSIP2X — Kit Contents

Circuit Breaker Mounting Shield Kit, I-Line IP2X

PowerPacT H, Quantity 1

PowerPacT J, Quantity 1

PowerPacT L, Quantity 1

Circuit Breaker

PowerPacT H, PowerPacT J, PowerPacT L

HNM4BLIP2X

4.5 in. Blank Filler I-Line IP2X

Quantity 3

Panelboard

HNM1BLIP2X

1.5 in. Blank Filler I-Line IP2X

Quantity 3

Panelboard

HLW4EBL

HLN1BL

HLN4BL

HLN4EBL

HLW4EBL

Blank extensions

Panelboard

Instruction Bulletin: 80030-695-02

HDTC

PowerPacT H Lugs shield

Circuit Breaker

Instruction Bulletin: 48044-002-04

JDTC

PowerPacT J Lugs shield

LGJTC

PowerPacT L Lugs shield

HJPA

PowerPacT H & J On/Off Fixed Padlock

Circuit Breaker

Instruction Bulletin: JYT65472

S32631

PowerPacT L On/Off Fixed Padlock

Circuit Breaker

Instruction Bulletin: 48049-246-02

HJBSW

PowerPacT H Mounting Bracket

Circuit Breaker

Instruction Bulletin: BQT94274

NOTE: Refer to the I-Line Circuit Breaker Power Distribution Panelboard Instruction Bulletin 80043-309-20.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?