DOCA0329EN-00

Firmware Update with EcoStruxure Power Commission Software

Use the latest version of EcoStruxure Power Commission software to:

  • Check the firmware compatibility of the devices in the intelligent modular unit (IMU).

  • Update the devices with the latest firmware version available.

After updating the firmware of one device, use EcoStruxure Power Commission software to check the firmware compatibility between IMU devices.

The Firmware Update table helps the user to diagnose and identify all discrepancy issues between IMU devices. This table also provides the recommended actions for each discrepancy issue.

Click here to download the latest version of EcoStruxure Power Commission software.

For more information about the use of EcoStruxure Power Commission software, refer to EcoStruxure Power Commission Online Help.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?