DOCA0329EN-00

BSCM Modbus SL/ULP Module

The BSCM Modbus SL/ULP module with commercial reference LV434220 is a Breaker Status Control Module that can be used with:

  • ComPacT NSX circuit breakers and switch-disconnectors

  • ComPacT NSX DC circuit breakers and switch-disconnectors

The BSCM Modbus SL/ULP module communicates data via:

  • Modbus Serial Line communication network

  • ULP communication network

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?