DUG_Wiser Micro Module Blind_CLP-00

Testing the device

Before using the module, manually test the module and make sure that it works when connected to the shutter.
  • Short press the push button once, the shutter opens/closes gradually.

  • Press and hold the push button, the shutter opens/closes fully, record the time it takes to fully open/close the shutter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.