Troubleshooting: Electrical Control Operations
Definition
Electrical control operations are operations that are made by an electrical order through a voltage release or by an external pushbutton that is directly connected to a voltage release.
Circuit Breaker Cannot be Closed by Using an External Pushbutton/Electrical Order
|
Symptom |
Probable causes |
Solutions |
|---|---|---|
|
– |
Circuit breaker is padlocked or keylocked in the open position. |
Unlock the circuit breaker. |
|
– |
Electrical closing order not executed by the XF closing voltage release due to insufficient voltage power supply. |
Check the voltage and the XF supply circuit (0.85–1.1 Un). If the problem persists, replace the XF closing voltage release. |
|
The closing spring and ready-to-close indicator shows that the mechanism is charged but the circuit breaker is not ready to close. |
MX opening voltage release is permanently powered. |
As there is an opening order, determine the origin of the order. The order must be canceled before the circuit breaker can be closed. |
|
MN undervoltage release is not powered due to an opening order. |
As there is an opening order, determine the origin of the order. The order must be canceled before the circuit breaker can be closed. |
|
|
MN undervoltage release is not powered due to insufficient voltage power supply. |
Check the voltage and the MN supply circuit (V > 0.85 Un). If the problem persists, replace the MN undervoltage release. |
Circuit Breaker Cannot be Opened by Using an External Pushbutton/Electrical Order
|
Probable causes |
Solutions |
|---|---|
|
Opening order is not executed by the MN undervoltage release. |
Drop in voltage insufficient or residual voltage (V > 0.35 Un) across the terminals of the MN undervoltage release. If the problem persists, replace the MN undervoltage release. |
|
Opening order is not executed by the MX opening voltage release. |
Check the voltage and the MX supply circuit (0.7–1.1 Un). If the problem persists, replace the MX opening voltage release. |
Additional Checks
If the troubleshooting actions described above do not work, refer to the troubleshooting information for Troubleshooting: Mechanical Control Operations.