DOCA0351EN-00

Locking the Switch-Disconnector in Open Position with Keylocks

Description

Optional keylocks can be used:

  • To lock one EasyPact MVS DA1 switch-disconnector in the open position. When locked, the switch-disconnector cannot be closed either locally with the closing pushbutton or remotely.

To use keylocks to lock the switch-disconnector in the open position, an optional OFF-position locking accessory is necessary.

VSPO OFF-Position Locking Accessory

The OFF-position locking accessory is an optional accessory that is mounted on the front of the switch-disconnector.

The OFF-position keylocking accessory can be fitted with one keylock.

The following type of keylock can be fitted:

Profalux keylock

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: MVS21736.

Locking the Switch-Disconnector in Open Position

Step

Action

1

Press and hold the opening pushbutton.

2

With the opening pushbutton pressed, turn the key clockwise to lock the switch-disconnector.

3

Remove the key.

4

Release the opening pushbutton.

5

Check that the switch-disconnector is locked in the open position and cannot be closed either locally with the closing pushbutton or remotely.

Unlocking the Switch-Disconnector

Step

Action

1

Put the key in the keylock.

2

Turn the key clockwise to unlock the switch-disconnector.

3

Press the closing pushbutton to close the switch-disconnector.

NOTE: The key remains captive in the keylock.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?