990-1000008A-001

Load Derating for UPS with IP31 Kit Installed

NOTICE
Risk of overheating
  • UPS with IP31 kit may have load deratings/temperature deratings/ overload deratings.
  • Read all instructions in the installation manual before installing or working on this UPS.
Failure to follow these instructions can result in equipment damage.
UPS rating

Maximum continuous load at 30 °C at power factor=1

Maximum continuous load at 35 °C at power factor=0.9

Maximum continuous load at 40 °C at power factor=0.9

250 kVA

200 kVA

212.5 kVA

200 kVA

300 kVA

240 kVA

255 kVA

240 kVA

400 kVA

320 kVA

340 kVA

320 kVA

500 kVA

400 kVA

425 kVA

400 kVA

600 kVA

480 kVA

510 kVA

480 kVA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.